Skip to main content
Brother Theo
Associate III
October 25, 2016
Question

I2S full duplex?

  • October 25, 2016
  • 1 reply
  • 543 views
Posted on October 25, 2016 at 18:12

Hi, I was trying to attach a AK4554 codec to a STM32F091CB using the SPI/I2S interface when I discovered it is half duplex only. I don't want to change to an F4 with an SAI interface if I can help it, as it is overkill and expensive. Is there a way to use both I2S half duplex channels to make one full duplex channel?

Thanks!

#codec-audio-i2s
This topic has been closed for replies.

1 reply

waclawek.jan
Super User
October 25, 2016
Posted on October 25, 2016 at 18:22

Yes - connect the clocks externally.

JW