Skip to main content
Fede Rico
Associate III
April 20, 2018
Question

USART Flow Control doesn't work on WiFi SPWF01SA

  • April 20, 2018
  • 0 replies
  • 493 views
Posted on April 20, 2018 at 09:00

Hi there,

I'm working on STM32F103 and a WiFi module SPWF01SA. I used the ST middleware and I can communicate with the WiFi module only without the Hardware Flow control.

I configured the USART1 with Flow Control using Cube32Mx

 huart1.Instance = USART1;
 huart1.Init.BaudRate = 115200;
 huart1.Init.WordLength = UART_WORDLENGTH_8B;
 huart1.Init.StopBits = UART_STOPBITS_1;
 huart1.Init.Parity = UART_PARITY_NONE;
 huart1.Init.Mode = UART_MODE_TX_RX;
 huart1.Init.HwFlowCtl = UART_HWCONTROL_RTS;
 huart1.Init.OverSampling = UART_OVERSAMPLING_16;�?�?�?�?�?�?�?�?

I copied this configuration from the example project. In fact this project use onlt the RTS pin.

I connected the WiFi CTS pin to the MCU RTS pin. and the WiFi RTS is unconnected.

The WiFi initialization works well until I send the command

status = SET_Configuration_Value(CONSOLE1_HWFC, 1);

After this command the WiFi module does not respond anymore.

Any suggestion?

Thanks for the help!

Federico

#hardware-flow-control #wifi-usart #spwf01
This topic has been closed for replies.