Skip to main content
Moamen Ayman
Associate III
July 29, 2017
Question

USB CDC library for stm32f042k6t6

  • July 29, 2017
  • 6 replies
  • 952 views
Posted on July 29, 2017 at 11:52

Hello, I am trying to use stm32f042k6t6 MCU and I want to use the USB peripheral implemented in it. Could someone suggest me a USB CDC library I can use with this MCU to connect with PC, I am using the standard peripheral libraries from ST so I am looking for a compatible CDC library. 

Thanks in advance.

    This topic has been closed for replies.

    6 replies

    Moamen Ayman
    Associate III
    July 29, 2017
    Posted on July 29, 2017 at 17:21

    I am trying to port this library to my IAR project and use the CDC library:

    https://my.st.com/content/my_st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32-standard-peripheral-libraries-expansions/stsw-stm32092.html

     

    I got many errors so what is the right functions to send data, receive data and get USB status?

    Vangelis Fortounas
    Associate II
    July 29, 2017
    Posted on July 29, 2017 at 22:42

    Hello!

    Yes you are right! errors.

    There is a good solution for making your USB functional.

    Try the

    https://my.st.com/content/my_st_com/en/products/development-tools/software-development-tools/stm32-software-development-tools/stm32-configurators-and-code-generators/stm32cubemx.html

    with HAL OR/AND LL drivers.

    This is not like StdPeriph_Driver but is compatible with IAR EWARM  and has also functional examples.

    Moamen Ayman
    Associate III
    August 1, 2017
    Posted on August 01, 2017 at 18:54

    Thanks Vangelis for your reply but I built the whole project based on the standard peripheral libraries so I want to use STSW-STM32092

    library

    this my code, I just want to initialize the CDC library and if any data received from the host, I send it back. does my code right?

    ♯ include 'usbd_cdc_core.h'

    ♯ include 'usbd_usr.h'

    USB_CORE_HANDLE USB_Device_dev ;

    extern USBD_Class_cb_TypeDef USBD_CDC_cb;

    int main(void)

    {

    USBD_Init(&USB_Device_dev, &USR_desc, &USBD_CDC_cb, &USR_cb);

    char data = 0;

    void *x = 0;

    USBD_CDC_cb.Init(x, 1);

    while (1)

    {

    if(USBD_CDC_cb.EP0_RxReady(x) == 1)

    {

    USBD_CDC_cb.DataIn(x, data);

    USBD_CDC_cb.DataOut(x, data);

    }

    }

    }

    Moamen Ayman
    Associate III
    August 1, 2017
    Posted on August 01, 2017 at 18:55

    Turvey.Clive.002

    Moamen Ayman
    Associate III
    August 1, 2017
    Posted on August 01, 2017 at 19:01

    Palmer.Randall

    Vangelis Fortounas
    Associate II
    August 1, 2017
    Posted on August 01, 2017 at 20:20

    Hello again!

    Inside  your USBD_CDC_cb structure  you put some callback functions  like   usbd_cdc_DataIn,  usbd_cdc_DataOut called when the appropriatre endpoind received or transmitted something.

    You can not use theese functions by calling them.

    Try to send from host , some  characters and observe theese callback functions how to behave.

    You can study also the example in STM32F0x2_USB-FS-Device_Lib V1.0.0\Projects\Virtual_COM_Port.