Skip to main content
hushel
Associate II
Jun 23, 2016 9:53 PM UTC
Question

Problems Calibrating Motion FX

Posted on June 23, 2016 at 23:53

I have read over the user manual for the MEMs board, and I am using the example code from the DataLogFusion. However, I can never get the osx_MotionFX_compass_isCalibrated function to return true. I have tried hitting the reset button, moving the board clockwise in all three axis, moving it in a figure 8 and lots of different combinations. 

Anyone have an idea how to do this successfully or what may be the problem? Thanks!
This topic has been closed for replies.

1 reply

louda.marian
ST Employee
Jul 1, 2016 2:14 PM UTC
Posted on July 01, 2016 at 16:14

Hello,

I don’t know which HW you are using, but try to check if all axes of all sensors (mainly ACC and MAG) are in the same direction. If not do the correction in your code.

Best Regards,

Marian