Skip to main content
jhousley
Associate II
July 26, 2016
Question

+WIND:5:WiFi Hardware Failure:5

  • July 26, 2016
  • 10 replies
  • 1772 views
Posted on July 26, 2016 at 19:08

I am consistently getting this error (+WIND:5:WiFi Hardware Failure:5) and I don't understand why? It is a pain because the module keeps having to be reset and it is impossible to communicate on a socket since this keeps happening. Any suggestions?

#spwf01sa #spwf01sa.11 #+wind:5
    This topic has been closed for replies.

    10 replies

    Gerardo GALLUCCI
    ST Employee
    July 27, 2016
    Posted on July 27, 2016 at 11:29

    Hi Jake,

    probably you are using an old FW release. Which version? Please update to FW3.5.

    Regards

    jerry

    jhousley
    jhousleyAuthor
    Associate II
    July 27, 2016
    Posted on July 27, 2016 at 20:46

    Hello Jerry,

    Thank you for getting back to me but I think I have the most up-to date version. I downloaded and installed the firmware off the website. When I so AT+S.STS I get the following for version:

    #  version = 160129-c5bf5ce-SPWF01S

    Which was released Jan-29 2016 I believe, Please let me know if that is correct. Thank you,

    -Jake

    Gerardo GALLUCCI
    ST Employee
    July 28, 2016
    Posted on July 28, 2016 at 08:48

    Hi Jake,

    FW you are using is already 3.5. Latest one.

    I'm not able to reproduce this issue since a lot of time. Can you share your setup (module variables, AP model, socket usage, other...)? It's interesting you are so ''lucky'' to get this error in a sistematic way! Did you already try to use another AP?

    If you want to speedup the process, contact your distributor, or ST support.

    Thanks

    jerry

    jhousley
    jhousleyAuthor
    Associate II
    August 1, 2016
    Posted on August 01, 2016 at 21:22

    Hello Jerry,

    It seems that I am getting this Error ever since I have started using this specific AP by my desk. Before I was using a different AP that was open with poor signal so I switched to this AP that was setup for me by my desk. When I try to open a socket either secure or just a TCP/UDP about every other time it will show up with this Hardware Failure error (sometimes while the socket is open). I checked the memory using free_heap and I have plenty of free memory even when doing SSL connections. The AP I am using is the Linksys E2500. We have to have our network setup very secure so it is invisible and the AP must know the devices Mac address that is connecting to it, which I have provided. My desktop is able to use the AP just fine so I don't know why I am consistently getting this error. Thank you,

    -Jake

    Gerardo GALLUCCI
    ST Employee
    August 2, 2016
    Posted on August 02, 2016 at 08:43

    Hi Jake,

    HW dead is not a RAM issue, and it's not a TCP/IP problem. I hope it's something happens during a network lost, or a disassociation, or something like this. Can you please share a full log, so I can take a look at console output before the failure?

    Please share also AT&V dump. Is AP set to b/g/n mode?

    Unfortunately I haven't this specific AP...

    Regards

    jerry

    jhousley
    jhousleyAuthor
    Associate II
    August 2, 2016
    Posted on August 02, 2016 at 18:05

    Hi Jerry,

    Attached is the terminal emulator output. I initially setup the connection with n mode enabled (I have tried it without and same results). The first thing I try is a PING and I get the Hardware Failure I then reset and try a sock connection and get a hardware failure. Please see attached. I want to note that when I switch to the other AP I can do PING and SOCK and secure SOCK and I have never gotten the hardware failure? Why is my desktop working with this AP and the module keeps getting Hardware failure? Thank you,

    -Jake

    ________________

    Attachments :

    HardwareFailure.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1Ro&d=%2Fa%2F0X0000000bn7%2FtfthJ6YqEokhNpoZrAbYyqEldXJiIY9ehM06g_MIkoE&asPdf=false
    Gerardo GALLUCCI
    ST Employee
    August 3, 2016
    Posted on August 03, 2016 at 10:48

    Hi Jake,

    thanks for the log. I've never seen an HW failure without a WIND:31 before. I have some hypothesis, but I cannot confirm without some debugging.

    Think I really need Linksys E2500 (N600, right?) to understand the root cause. Hope to find it. Otherwise, are you already in touch with ST offices, or distributor...?

    Regards

    jerry

    mafredri
    Associate II
    November 2, 2016
    Posted on November 02, 2016 at 18:42

    I've also experienced WIND 5 (Hardware Failure 5) so I thought I would share my report on the issue.

    I've tested the SPWF01SA Wi-Fi module in a area with high Wi-Fi congestion, connected to a Meraki network and have experienced connectivity problems.

    When the Wi-Fi module is connected to the Meraki network it occasionally stops responding to ping (ping from computer to SPWF01SA module). Sometimes it does not respond for 20 seconds, but usually it starts responding some time after that (if doing no other interaction to with the module).

    However, if I issue a HTTP GET request during the time that the module does not respond to ping, the module goes into a state where it stops responding at all.

    Example:

    AT+S.HTTPGET=10.0.0.100,/,8080

    ~8 minutes later

    ERROR: nothing received, increase ip_http_get_recv_timeout variable

    +WIND:5:WiFi Hardware Failure:5

    This issue seems to appear when the Wi-Fi module is in normal operation (AT+CFUN=0), whereas it does not seem to happen in power save mode (AT+CFUN=2). It also does not seem to matter if 802.11n operation is enabled or not, the issue is still present.

    Reproduction steps:

    1. Connect Wi-Fi module to Meraki network

    2. Start pinging the Wi-Fi module

    3. Wait until the Wi-Fi module stops responding to ping

    4. Issue HTTP GET request

    5. Wi-Fi module stops responding (eventual HW failure)

    The HTTP GET is not mandatory for HW Failure, it just speeds up the process.

    This problem did not occur previously in an area with less Wi-Fi congestion (at least not to this degree).

    Also, I'm not 100% sure, but I can't recall having this problem before updating from FW v3.3, but it is very easy to reproduce on FW v3.4 and v3.5.

    I have done limited testing with a different AP in this location (TP-LINK MR3020) and have so-far not been able to reproduce the issue fully (there is only one ping loss on occasion). Potentially interesting fact is that the Wi-Fi communication happens faster on the Meraki network compared to MR3020 as can be seen in the following ping test.

    100 pings on MR3020:

    100 packets transmitted, 99 packets received, 1.0% packet loss

    round-trip min/avg/max/stddev = 2.362/14.243/135.907/22.386 ms

    100 pings on Meraki:

    100 packets transmitted, 99 packets received, 1.0% packet loss

    round-trip min/avg/max/stddev = 1.772/4.189/27.654/4.250 ms

    I'm wondering if there can be a potential race condition in the SPWF01SA firmware when the Wi-Fi communication is too fast?

    Gerardo GALLUCCI
    ST Employee
    February 4, 2017
    Posted on February 04, 2017 at 11:30

     ,

     ,

    Up this thread!

    Both problems have been reproduced. Fix is under testing.

    Problem ♯ 1: Hardware Failure + WiFi Exception. It's confirmed that CFUN=2 (radio in powersave) has not this problem.

    Problem ♯ 2: Hardware Failure

    Thanks to mf and jake

    ciao

    j

    Muhammad Usman
    Visitor II
    March 28, 2018
    Posted on March 28, 2018 at 10:03

    Hi Gerardo Gallucci,

    I am having the same problem, but I couldn't find any new release after 11/01/2017.

    Can you please help me out?