Skip to main content
pontus2
Associate II
August 12, 2016
Question

Module UART RX buffer

  • August 12, 2016
  • 1 reply
  • 562 views
Posted on August 12, 2016 at 08:17

I cannot find information on the SPWFS01 UART RX buffer. How big is it? Since I have an issue when controlling the SPFWS01 from a host using UART. We have a cycle where we use HTTPREQ and in there use GET, PUT and then DELETE. Since the PUT also contains more headers and a body this message is a lot larger than the other ones but it is within the limits of my buffers (both HW and SW). However this AT+HTTPREQ with PUT works 49/50 times with the one erronous time being when the HOST is not able to transmit more than its first character. We are using HWFC and 38,4k.

Any ideas? 
    This topic has been closed for replies.

    1 reply

    Gerardo GALLUCCI
    ST Employee
    August 23, 2016
    Posted on August 23, 2016 at 21:19

    Buffer is 2K in size. HW flow control ensures data not lost during upload stage.

    Be sure to transmit next AT+HTTPREQ after previous ending (OK or ERROR)