Skip to main content
eric239955_stm1_stmicro
Associate II
June 30, 2016
Question

STM32F4 TIM1 DMA CCR1

  • June 30, 2016
  • 2 replies
  • 965 views
Posted on June 30, 2016 at 21:57

I plan to use the STM32F40x TIM1 CH1 (PA8) to produce a varying  PWM  signal. The base frequency is set, say 1 MHz.  I need to use DMA to change the PWM duty cycle on every iteration. I know this can be done by aiming the DMA at the TIM1_CCR1 register, but the question is which DMA stream to use. 

The STM32F4xx Reference Manual (R12, May 2016) Table 43 says that DMA2 Channel 6, Stream 1 and Stream3 are both associated with TIM1, but which is the right one for the CCR1 register?

I know that you program the address of the TIM1 CCR1 register into the appropriate DMA control registers, but that the correct stream has to be used so that the TIM1 PWM generation mechanism knows to notify the right DMA channel/stream when it is ready for the next value.

#dma #tim1 #stm32f4
This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
June 30, 2016
Posted on June 30, 2016 at 23:21

So either would work, the Channel is an input mux to the Stream. The DMA Unit supports 8 unique streams (akin to channels on IBM PC architectures of yore, and textbook examples)

Purpose of having choices is that you can pick the mix of DMA to support all the peripherals you use.

I'd lean to using the Update as a trigger, as it occurs once per period instead of potentially chasing the phase of the counter.

TIM1_UP would be DMA2 Stream 5 Channel 6

You'd write to &TIM1->CCR1, it would be a Half-Word (16-bit)

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Tesla DeLorean
Guru
June 30, 2016
Posted on June 30, 2016 at 23:24

Example of 32-bit TIM5 CH1 on APB1(DMA1), in case this saves me recreating the wheel

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F4%20DMA%20and%20Varying%20Duty%20Cycle&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx&currentviews=53]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex%5fmx%5fstm32%2fSTM32F4%20DMA%20and%20Varying%20Duty%20Cycle&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex%5Fmx%5Fstm32%2FAllItems%2Easpx¤tviews=53

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..