Skip to main content
rsharifi9
Associate III
October 29, 2017
Question

discovery f746 I/O pins not accessible?

  • October 29, 2017
  • 2 replies
  • 693 views
Posted on October 29, 2017 at 11:09

hi Everybody,

in the discovery F746 board, the I/O pins are not accessible?

regards, Ras

#discovery-f746
    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    October 29, 2017
    Posted on October 29, 2017 at 11:22

    Most everything is committed to a specific purpose. The Arduino shield socket is best means of expansion / exposure of available signals.

    Use the NUCLEO-144 if you need a breakout board.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    S.Ma
    Principal
    October 29, 2017
    Posted on October 29, 2017 at 11:26

    Discovery board implement built-in feature of components requirering high speed signals which wouldn't survive well through a connector (DSI, USB, SDRAM, QSPI, uSD), left pins are the one going through connectors, and as Clive said, Arduino is the prime access to some GPIOs. On newer discovery kits, you may find more GPIO accessible through PMOD/STMod+ connectors (which are feature rich GPIOs), making the discovery kits a bit closer to Nucleo's.