Question
Getting started with stm3210e-EVAL
Posted on June 28, 2016 at 10:34
Hi everybody,
I am trying to use the stm3210e-eval with IAR (7.70). I have downloaded the demonstration software and followed the readme instructions. - EWARM - Open the STM3210E-EVAL_Demo.eww workspace - Rebuild all files: Project->Rebuild all - Load project image: Project->Debug - Run program: Debug->Go(F5) When I launch the debug, I have a fatal error ''Cannot connect to J-Link via USB''. The board is connected as USB and the screen and the LEDs are On but I do not see the board in the Windows device manager so I am not sure it is well detected although I installed the USB driver STSW-LINK009 is installed. Does someone know how to fix the problem ? Thanks very much for your help :)