Skip to main content
sergeyvslnko
Associate II
January 16, 2018
Question

LSM9DS1. DRDY_M pin

  • January 16, 2018
  • 6 replies
  • 2337 views
Posted on January 16, 2018 at 11:10

In the datasheet say that this pin must be work(indicate moment of magnetometer new data avalaible ) automatically(without need of configuration), but it doesn't work. Why?

In the

http://www.st.com/resource/en/datasheet/iis2mdc.pdf

said that M_XYZ_DA status bit must be connected with DRDY_M output pin(page 32,

CFG_REG_C (62h) 0 bit

).

D

oes not LSM9DS1 datasheet contain complete information?

This question(

https://community.st.com/0D50X00009XkhX7SAJ

) has proved this  assumption

null
This topic has been closed for replies.

6 replies

ST Employee
January 17, 2018
Posted on January 17, 2018 at 12:39

The DRDY_M signal is available without any configuration.

Do you read the data from the magnetometer? If not the DRDY is set and stay high until you read the data.

sergeyvslnko
Associate II
January 17, 2018
Posted on January 17, 2018 at 13:50

After magnetometer initialization DRDY_M set up to HIGH. When I first read mag data it set to LOW and... it was staying LOW until power reset action

in spite of

magnetometer data were correctly read again and again.

I have decided this issue when change configuration value of

CTRL_REG3_M (22h)

register from 0x84 to 0x04(7th

bit setting disable I2C interface

).

How I2C interface is connected with DRDY_M signal?

PS

Batek.Miroslav

, thank you,

your attention helped to solve this problem

.

ST Employee
January 17, 2018
Posted on January 17, 2018 at 14:16

Do you want to say that the DRDY_M stop work when you set CTRL_REG3_M (22h) to 0x04 and it works if the value is 0x84?

I'm not able replicate this issue.