Question
DAC waveform not displaying on oscilloscope.
Posted on July 12, 2016 at 04:56
Hi ST community,
I'm doing a feedback of the adc output to the dac input to double check the incoming signal. I seem to have a problem displaying the DAC(PA5) waveform on the oscilloscope, so my setup is : i connect the function generator output of 800hz to the input of the ADC(PA0) & GND of func. generator is connected to GND on the stm32f429i discovery board. However, when i put a oscilloscope probe to the DAC(PA5) the waveform shows, but then when i connect the osclloscope's gnd to the board's gnd, the signal flatlines and no waveform appears. May i know if anyone has faced this issue before? #adc #stm32 #discovery #dac