Skip to main content
dieter 123
Associate III
September 7, 2017
Question

bug in STM32 LWIP in IAP example?

Posted on September 07, 2017 at 08:07

could it be that in STM32Cube_FW_F4_V1.16.0\Projects\STM324xG_EVAL\Applications\LwIP\LwIP_IAP

the latest firefox is not supported?

FW download via internet explorer works but but not firefox 55.0.3 (32-Bit) !

Thx

    This topic has been closed for replies.

    2 replies

    dieter 123
    Associate III
    November 22, 2017
    Posted on November 22, 2017 at 10:10

    HAJJEM.Oussema

    Can you comment on this issue?

    The ST is code in this project is meant to work with firefow as well. But it doesnt!

    Same applies to google chrome browser

    Is ST going to fix this?

    Oussema Hajjem_O
    Visitor II
    November 23, 2017
    Posted on November 23, 2017 at 10:58

    Hello,

    I confirm that some regressions are available when using last Firefox versions, this will be reported to be fixed in the next STM32CubeFW F4 releases.

    Thanks and regards,

    Oussema.