issue about stm32l431 rtc second register update
hi,i initialize and set rtc as follow
int rtcInit(void){
RCC->APB1ENR1 |= RCC_APB1ENR1_PWREN; // enable PWR clock
PWR->CR1 |= 0x00000100; // disable BD write protect while(0 == (PWR->CR1 & 0x00000100)); RCC->BDCR |= ((1 << 15) | (3 << 8)); // enable RTC clock,select HSE/32 as clock source of rtc,HSE is 8M PWR->CR1 &= 0xFFFFFEFF; // enable BD write protect RCC->APB1ENR1 &= ~(RCC_APB1ENR1_PWREN); // disable PWR clockreturn 0;
}int rtcSet(unsigned short year,unsigned char month,unsigned char day,unsigned char hours,unsigned char minute,unsigned char second,unsigned int mSecond){
RCC->APB1ENR1 |= RCC_APB1ENR1_PWREN; // enable PWR clock
PWR->CR1 |= 0x00000100; // disable BD write protect while(0 == (PWR->CR1 & 0x00000100)); RTC->WPR = 0xCA; RTC->WPR = 0x53; // disable rtc write protect RTC->CR = 0x00000000; RTC->ISR |= (1 << 7); // enter initialize mode while (0 == (RTC->ISR & (1 << 6))); // wait for enter initialize mode RTC->PRER = (124 << 16) | (1999 << 0); // rtcSrcClock is HSE/32 = 250000 RTC->TR = (((hours/10)%10) << 20) | ((hours%10) << 16) | (((minute/10)%10) << 12) | ((minute%10) << 8) | (((second/10)%10) << 4) | ((second%10) << 0); RTC->DR = (((year/10)%10) << 20) | ((year%10) << 16) | (((month/10)%10) << 12) | ((month%10) << 8) | (((day/10)%10) << 4) | ((day%10) << 0); RTC->ISR &= ~(1 << 7); // exit initialize mode PWR->CR1 &= 0xFFFFFEFF; // enable BD write protect RCC->APB1ENR1 &= ~(RCC_APB1ENR1_PWREN); // disable PWR clock return (0 == (RTC->ISR & (1 << 4)));}int rtcGet(unsigned short * year,unsigned char * month,unsigned char * day,unsigned char * hours,unsigned char * minute,unsigned char * second,unsigned int * mSecond){
unsigned int rtcd,rtct,rtcss,rst;
if((NULL == year) || (NULL == month) || (NULL == day) || (NULL == hours) || (NULL == minute) || (NULL == second) || (NULL == mSecond)) { logWarnFL(''invalid argument %p %p %p %p %p %p %p\r\n'',year,month,day,hours,minute,second,mSecond); return -1; } if(0 == (RTC->ISR & (1 << 4))) { // RTC not initialize logWarnFL(''rtc not initialize\r\n''); return -2; }RTC->ISR |= (1 << 5); // clear RSF
while (0 == (RTC->ISR & (1 << 5))); // wait for RSF assert RTC->ISR |= (1 << 5); // clear RSF rtct = RTC->TR; rtcss = RTC->SSR; rtcd = RTC->DR; rst = RTC->SSR & (1 << 5);*year = ((rtcd >> 20) & 0x0F) * 10 + ((rtcd >> 16) & 0x0F) + 2000;
*month = ((rtcd >> 12) & 0x01) * 10 + ((rtcd >> 8) & 0x0F); *day = ((rtcd >> 4) & 0x03) * 10 + ((rtcd >> 0) & 0x0F); *hours = ((rtct >> 20) & 0x03) * 10 + ((rtct >> 16) & 0x0F); *minute = ((rtct >> 12) & 0x07) * 10 + ((rtct >> 8) & 0x0F); *second = ((rtct >> 4) & 0x07) * 10 + ((rtct >> 0) & 0x0F); *mSecond = (2000 - rtcss)/2; return rst;}void rtcPrint(void){
unsigned short year;
unsigned char month,day,hours,minute,second; unsigned int mSecond; int rst = rtcGet(&year,&month,&day,&hours,&minute,&second,&mSecond);logInfo(''%02d-%02d-%02d %02d:%02d:%02d %03d ----> %d\r\n'',year,month,day,hours,minute,second,mSecond,rst);
return;}then i initialize it
...
rtcInit();
rtcSet(2017,1,10,12,0,0,0)
finally,i print date and time on a dead-loop
while(1) { int i = 0x1FFFFF;while(i--); rtcPrint(); }
as follow