Skip to main content
Elwood Downey
Associate III
June 27, 2017
Question

STLink reports: The interface firmware FAILED to reset/halt the target MCU

  • June 27, 2017
  • 0 replies
  • 478 views
Posted on June 27, 2017 at 22:08

I developed the code for my application using Nucleo F446Ze. I use CubeMX and gcc on macOS. All works fine.

Next I want to develop my own PCB with the same processor. Thinking ahead to how I will flash it, I broke off the STLINK and practiced connecting it up back to the Nucleo and programming with the SWD connector (CN6 on the STLINK). This also works fine so I think I know how to connect with the STLINK.

I now have my new PCB. Voltages look good. Current draw is 14 mA. I connect the same STLINK but it does not work. The multi-color LED is Red and never blinks. After copying the bin file to the mounted STLINK file system the following message appears in FAIL.TXT: The interface firmware FAILED to reset/halt the target MCU.

Can anyone expand on exactly what this means? I agree it is probably my new board but I do not know where to start looking.

Thank you.

    This topic has been closed for replies.