Skip to main content
john1389
Associate
July 22, 2016
Question

Is interbal RC Osc accurate enough for serial UART TS232 for STM32F103RB?

  • July 22, 2016
  • 2 replies
  • 708 views
Posted on July 22, 2016 at 22:31

Is it true that 2 to 3% accuracy is required? 

Nucleo F103 has no crystal. Nucleo F401 has 32kHz crystal
    This topic has been closed for replies.

    2 replies

    waclawek.jan
    Super User
    July 22, 2016
    Posted on July 22, 2016 at 23:12

    > Is it true that 2 to 3% accuracy is required? 

    Yes.

    JW

    Tesla DeLorean
    Guru
    July 22, 2016
    Posted on July 23, 2016 at 01:14

    Both Nucleo boards can take an 8 MHz clock source from the ST-LINK chip which does have an HSE clock.

    USARTs can tolerate a fair amount of clock error.

    The LSI is not only likely to be off in frequency, but it also changes (poor stability). Can't say I've spent a lot of time looking at the HSI, but have got some boards wired to a GPS 1PPS source so could probably evaluate it.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..