Question
To develop Command for Servo MOTOR (motion control)
Posted on July 29, 2016 at 17:13
Hi,
I am new in STM32.I want to develop controller with 2 independent pulse train or specific amount of pulse output with 50% fixed duty cycle. In project i want all the command to be added which in dspin project same type command to develop.command like :-MOVE, ACCEL, DECEL, SPEED. POSITION, MARK, MARK POSITION same all as in dspin.Need help in PWM control, like want to send 2K pulse and then PWM to stop.Min pulse 1 Hz to Max pulse 1 Mhz.Kindly guide me, i any one is having any reference code.I am using STM32F discovery board.Thanks and Regards,Pankaj