2018-02-26 3:00 AM
hi i am kalpesh , i new in stm8 . I want to learn how to program in stm8. Please tell me which software should i use?
please help me . i have Stm8s003f3 20pin IC .
i search @ internet i didn't get ?
please help me?
sorry for poor english
thank you
2018-02-26 11:52 AM
Here are two simple tutorials for the STM8S003F3:
http://colecovision.eu/stm8/STM8%20Min%20Sys%20Dev%20LED.shtml
http://colecovision.eu/stm8/STM8%20Min%20Sys%20Dev%20Serial.shtml
Both use SDCC for the compiler.
Philipp
2018-03-28 7:31 AM
Take a look at this simple example that blinks the LED in the STM8S-DISCOVERY board using Timer TIM1. The code is written for a different MCU (STM8S105C6), but it is easy to port to STM8S003F3. You could use IAR or COSMIC+STVD as IDE. There are links on the GitHub README file and the code is ported for both.
2018-05-14 3:30 AM
thank you . i will go through it.
2018-05-18 11:06 PM
Hi
I am lokesh.
kalpesh use IAR id for stm8.
very simple ,easy to use, easy for debugging.
IAR provide free version for 8kb memory limit.
i also attach a youtube channel link .
which provide all pheripheral video like gpio toggle , timer , external interrupt and etc.
https://www.youtube.com/channel/UCMnrf_QCcGwOv_TdvHxtTQQ/playlists