Skip to main content
w21685
Associate II
October 7, 2016
Question

Regarding Flash memory Read/Write

  • October 7, 2016
  • 2 replies
  • 715 views
Posted on October 07, 2016 at 16:32

Hello,

I'm using a STM32F207 series.

I was wondering about the flash memory read/write/earse as EEPROM.

Do I have to Erase the flash memory every time before writing a data?

Thanks.

    This topic has been closed for replies.

    2 replies

    matic
    Associate III
    October 7, 2016
    Posted on October 07, 2016 at 17:18

    Hi.

    You can program Flash by half-word each time. Location must be erased before programming. (erased state is 0xFFFF). If it is not, warning bit in FLASH->SR register is set. One exception is when you can program a non-erased location - this is when you program 0x0000. Regardless previous state, the location will be programmed to 0x0000.

    Regarding to your question. No, it is not necessary to erase the whole page before programming. Just make sure that a location where you want to write is erased (0xFFFF).

    w21685
    w21685Author
    Associate II
    October 23, 2016
    Posted on October 23, 2016 at 20:03

    Thank you for your reply!