Skip to main content
luigi2399
Visitor II
September 1, 2016
Question

BlueNRG Read Advertising Data

  • September 1, 2016
  • 0 replies
  • 463 views
Posted on September 01, 2016 at 17:00

How I can read adversising data after a scanning ?

I use this instruction for scanning:

/////////////////////////////////////////////////////////////////////////////////

//

// Fa partire l' advertising

//

static int BleStartScanning(void)

{

    uint16_t service_handle, dev_name_char_handle, appearance_char_handle;

    int status = 0;

    // Reset

    BlueNRG_RST();

    // Set Address

    if((status = aci_hal_write_config_data(CONFIG_DATA_PUBADDR_OFFSET, CONFIG_DATA_PUBADDR_LEN,    m_MacAddress_Client)) != 0){

        return status;

    }

    uint8_t role[] = {0x01};

    if((status = aci_hal_write_config_data(CONFIG_DATA_ROLE, 0x01, role)) != 0){

        return status;

    }

    // Inizializza livello GATT

    if((status = aci_gatt_init()) != 0){

        return status;

    }

    if (m_bnrg_expansion_board == IDB05A1) {

        status = aci_gap_init_IDB05A1(GAP_CENTRAL_ROLE_IDB05A1, 0, 0x07, &service_handle, &dev_name_char_handle, &appearance_char_handle);

    }  else {

        status = aci_gap_init_IDB04A1(GAP_CENTRAL_ROLE_IDB05A1, &service_handle, &dev_name_char_handle, &appearance_char_handle);

    }

    if(status != 0){

        return status;

    }

    if((status  =aci_gap_start_general_discovery_proc(0x0800, 0x0036,PUBLIC_ADDR, 0x00)) != 0){

        return status;

    }

    return status;

}

After scannig I receive the event :

EVT_LE_ADVERTISING_REPORT

but in this event there is only address data e not aadversting Data.

How I can read this data before start  connecting procedure ?

Thanks

This topic has been closed for replies.