Skip to main content
DarkTaipei
Associate II
September 16, 2016
Solved

STM32CubeMX setting for STM32F7 SPI

  • September 16, 2016
  • 5 replies
  • 1941 views
Posted on September 17, 2016 at 00:56

Hi,

I used to work on STM32F4 and now are evaluating STM32F7. When I tried to create a project with STM32F769NI with SPI. I found that I can't set the Prescaler to 2 (APB2 = 108Mhz) which will result the SPI6 to 54Mhz.

The error message is ''With this Prescaler value and APB2 Clock Frequency (108.0 MHz), Baud Rate is more than : 50.0 MBit/s. 

But the datasheet clear said it can go up to 54MHz. So..

The program is wrong, datasheet is wrong or I am wrong? (SPI 6, master mode with full duplex). I also set the voltage to 3.3. 

Regards,

TYY

#stm32f7-spi
This topic has been closed for replies.
Best answer by stm32cube-t
Posted on January 02, 2017 at 16:15

Original issue has been fixed in 4.18 release: 'With SPI on STM32F769NI, set the Prescaler to 2 (APB2 = 108Mhz), set the voltage range to 3.3 V. With this Prescaler value and APB2 Clock Frequency (108.0 MHz), maximum Baud Rate is 50.0 MBit/s when we should be able to reach SPI6 at 54Mhz'.

Indeed:

 - The max value depends on voltage range. So 54MHz, should be proposed if application is running 3.3V typical.

- At low voltage range, the delay on the pad is longer and limits the max frequency.

5 replies

slimen
Visitor II
September 19, 2016
Posted on September 19, 2016 at 15:49

Hi,

Could you precise which version of CubeMx are you using ?

Regards

Nesrine M_O
Associate
September 19, 2016
Posted on September 19, 2016 at 15:52

Hi TONYY,

Could you please precise which CubeMX version are you using?If you are using an old version, I recommend you to use the latest: 4.16.1

-Syrine-

Nesrine M_O
Associate
September 20, 2016
Posted on September 20, 2016 at 10:45

Hi TONYY,

Thank you for your feedback. The issue has been reported internally.

-Syrine-

stm32cube-t
stm32cube-tBest answer
ST Employee
January 2, 2017
Posted on January 02, 2017 at 16:15

Original issue has been fixed in 4.18 release: 'With SPI on STM32F769NI, set the Prescaler to 2 (APB2 = 108Mhz), set the voltage range to 3.3 V. With this Prescaler value and APB2 Clock Frequency (108.0 MHz), maximum Baud Rate is 50.0 MBit/s when we should be able to reach SPI6 at 54Mhz'.

Indeed:

 - The max value depends on voltage range. So 54MHz, should be proposed if application is running 3.3V typical.

- At low voltage range, the delay on the pad is longer and limits the max frequency.