Associate
September 30, 2016
Question
Unable to run program on STM32F091VB
- September 30, 2016
- 3 replies
- 1041 views
Posted on September 30, 2016 at 11:59
Hi,
I programmed simple GPIO high/low code on STM32F091VB through STVP but not getting any output from it. First, i configured BOOT OPTION BYTE then i was able to flash the microcontroller successfully. Refer attachment for option byte configuration.I checked my program and hardware, it doesn't seems to have any problem.I think STM32F091VB is not executing program in current configuration. Plz suggest if there is any config. for boot and other thing. #stm32f091vb