Jump to another application in Flash memory on stm32f4-discovery board
How to jump to another application in Flash memory on stm32f4-discovery board? Can anyone give complete ibstruction step by step? I have already written bin file to flash. Now I want only to run it. I looked through manu forums and saw a lot of advises, but my project doesn't work.
It is one of the examples I've seen:
static void boot_jump(uint32_t address) {
typedef void (*pFunction)(void);pFunction Jump_To_Application;uint32_t JumpAddress;if (((*(__IO uint32_t*)ApplicationAddress) & 0x2FFE0000 ) == 0x20000000) { JumpAddress = *(__IO uint32_t*) (ApplicationAddress + 4); Jump_To_Application = (pFunction) JumpAddress; __set_MSP(*(__IO uint32_t*) ApplicationAddress); Jump_To_Application(); }}It is in first default application. And In another target application I modified file system_stm32f4xx.c:
#define VECT_TAB_SRAM
#define VECT_TAB_OFFSET 0x10000 /*!< Vector Table base offset field. This value must be a multiple of 0x200. */I also modified options for Target-Target IROM1: 0x8010000 SIze 0x8000
and Linker: Disable 'Use Memory Layout from Target Dialog' and R/O Base:0x8010000