Skip to main content
troky
Associate
October 11, 2016
Solved

CR95HF Ultralight-C problem

  • October 11, 2016
  • 1 reply
  • 751 views
Posted on October 11, 2016 at 15:14

Hello,

I am having problems with UL-C authentication command (0x1A 0x00). CR95HF always responds with 0x87 (timeout) instead of 0xAF. Beside that everything else works fine.

Does anyone have working code for authenticating UL-C?

Sanjin
    This topic has been closed for replies.
    Best answer by Peter Boringer
    Posted on October 17, 2016 at 17:28

    Dear Sanjin,

    If you have the return code  0x87 I think that the TAG has not understood the request and thus has not provided any answer. I suggest you to check the TAG provider specifications in order to tune the command sent to the TAG for the Authenticate process.

    From my knowledge the CR95HF in native is not able to perform this process as it includes proprietary commands and specific secured algorithms. To execute it you can try to adapt it via SW using the CR95HF send receive commands.

    Hope it will help

    Regards

      

    1 reply

    Peter Boringer
    Peter BoringerBest answer
    Visitor II
    October 17, 2016
    Posted on October 17, 2016 at 17:28

    Dear Sanjin,

    If you have the return code  0x87 I think that the TAG has not understood the request and thus has not provided any answer. I suggest you to check the TAG provider specifications in order to tune the command sent to the TAG for the Authenticate process.

    From my knowledge the CR95HF in native is not able to perform this process as it includes proprietary commands and specific secured algorithms. To execute it you can try to adapt it via SW using the CR95HF send receive commands.

    Hope it will help

    Regards