Skip to main content
francisco
Associate
October 11, 2016
Question

BLDC faults using Motor Control Library (FOC SDK v4.2)

  • October 11, 2016
  • 2 replies
  • 655 views
Posted on October 11, 2016 at 11:31

Hello everybody,

I am trying to run a BLDC motor with the FOC SDK v4.2, using a STEVAL-IHM021V2 power stage and STMF32F303RE Nucleo board as MCU.

I set everything up with no trouble and connect the board to MC Workbench, but when I click start the motor shivers and stops. If I use Hall sensors, I receive a Speed Feeback fault, while sensorless I get a Start-up fault.

I believe they are both originated by the same issue: the low sides for U and W are always triggered simultaneously. I have revised the connections and they are not mutually connected. Did someone have the same problem? Any solutions/suggestions?

Thanks in advance,

Francisco

#pmsm-foc-stm32f3 #stm32f303 #nucleof303
This topic has been closed for replies.

2 replies

ba_it
Visitor II
December 12, 2016
Posted on December 12, 2016 at 17:31

Hi Francisco. I have similar problem usinf STEVAL-IHM034V2 and a PMSM motor with sensorless control. I solve this changing the PID parameters, but I also not able to increase the motor speed.

Walid FTITI_O
Visitor II
December 13, 2016
Posted on December 13, 2016 at 11:45

Hi 

I recommend your hardware an software setup by referring to the user manual

http://www.st.com/content/ccc/resource/technical/document/user_manual/c5/b5/50/ee/3b/b9/46/b0/DM00041947.pdf/files/DM00041947.pdf/jcr:content/translations/en.DM00041947.pdf

-Walid F-