Skip to main content
_dalbert
Associate II
October 11, 2016
Question

STM32L051 PLL limit with HSI

  • October 11, 2016
  • 1 reply
  • 702 views
Posted on October 11, 2016 at 21:00

Using an STM32L051, I am unable to generate a 32MHz system clock from from the PLL using the HSI as the clock source.  I can generate up to 24MHz without trouble, but any attempt to generate higher frequencies results in the system locking up.

This code fails:

    // Select internal 16MHz RC oscillator divided by 4 as clock source

    RCC->CR |= RCC_CR_HSION | RCC_CR_HSIDIVEN;

    // Wait for HSI ready

    while (!(RCC->CR & RCC_CR_HSIRDY));

    // Enable PLL with HSI as source

    RCC->CFGR &= ~RCC_CFGR_PLLSRC_HSE; // set PLL source to HSI

    RCC->CFGR |= RCC_CFGR_PLLMUL24 | RCC_CFGR_PLLDIV3;

    RCC->CR   |= RCC_CR_PLLON;

    // Wait for PLL ready

    while (!(RCC->CR & RCC_CR_PLLRDY));

    // Change system clock to PLL

    RCC->CFGR = (RCC->CFGR & ~RCC_CFGR_SW) | RCC_CFGR_SW_PLL;

    // Update SystemCoreClock to reflect new speed

    SystemCoreClockUpdate();

If you change PLLDIV3 to PLLDIV4, it works, but at 24MHz.

I have tried a wide range of multipliers and divisors, but the limit always seems to be 24MHz.  Is this a known issue?  If so, it is not in the errata.

#stm32l0-pll
This topic has been closed for replies.

1 reply

_dalbert
_dalbertAuthor
Associate II
October 11, 2016
Posted on October 11, 2016 at 22:46

I found the answer, leaving it here for anyone else who encounters the same problem:

Flash requires 1 wait state when running above 24MHz, so adding this fixes the problem:

FLASH->ACR |= FLASH_ACR_LATENCY;