Skip to main content
mario_fischer
Visitor II
October 18, 2016
Question

Problems with internal bootloader on STM32F405

  • October 18, 2016
  • 1 reply
  • 625 views
Posted on October 18, 2016 at 14:40

We use the internal bootloader of the controller to do the initial firmware programming via USB (DFU). In the last time the we run into trouble with some units - the devices don't properly enumerate on USB (unknown device).

The hardware seems to be ok, since once programmed with our own firmware via SWD, the devices running fine.

I tried to debug the internal bootloader, but didn't come close to a meaningful cause. What I've seen is an endless loop starting nearby 0x1FFF369C, that obviously checks the USART1/3 and the CAN related GPIO Pins. The PLL still uses the HSI clock.

We tied all the CAN and USART related pins according to AN 2606 to a fixed level.

Can somebody give me a hint regarding the cause of this behavior.

#bootloader
This topic has been closed for replies.

1 reply

Tesla DeLorean
Guru
October 18, 2016
Posted on October 18, 2016 at 16:18

Make sure your HSE crystal starts quickly, and stabilizes to the correct frequency. The loader expects a number of specific frequencies which it benchmarks. Evaluate in your app. Try also a VCP/MSC USB load on your board, does that function properly?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..