Skip to main content
martonmiklos
Senior
September 15, 2017
Question

[CubeMX feature request]Prevent warning when using custom USB String descriptors

Posted on September 15, 2017 at 13:34

If I setup custom string USB string descriptors in the CDC Middleware configuration...

0690X00000608FwQAI.png

..these strings will be generated to the usbd_desc.c file in the following format:

/** @defgroup USBD_DESC_Private_Defines
 * @{
 */ 
#define USBD_VID 1155
#define USBD_LANGID_STRING 1033
#define USBD_MANUFACTURER_STRING ''Digitroll Ltd.''
#define USBD_PID_FS 22336
#define USBD_PRODUCT_STRING_FS ''XLiNE-USB Converter''
#define USBD_SERIALNUMBER_STRING_FS ''00000000001A''
#define USBD_CONFIGURATION_STRING_FS ''CDC Config''
#define USBD_INTERFACE_STRING_FS ''CDC Interface''�?�?�?�?�?�?�?�?�?�?�?

When compiling this code with gcc I got the following warnings:

pointer targets in passing argument 1 of 'USBD_GetString' differ in signedness [-Wpointer-sign] usbd_desc.c /xlineusb/Src line 76 C/C++ Problem�?

It is because the the USBD_getString expects unsigned pointer:

void USBD_GetString (uint8_t *desc, uint8_t *unicode, uint16_t *len);�?

I would recommend to generate the USB descriptor strings in the following format to prevent these warnings:

/** @defgroup USBD_DESC_Private_Defines
 * @{
 */ 
#define USBD_VID 1155
#define USBD_LANGID_STRING 1033
#define USBD_MANUFACTURER_STRING (uint8_t*)(''Digitroll Ltd.'')
#define USBD_PID_FS 22336
#define USBD_PRODUCT_STRING_FS (uint8_t*)(''XLiNE-USB Converter'')
#define USBD_SERIALNUMBER_STRING_FS (uint8_t*)(''00000000001A'')
#define USBD_CONFIGURATION_STRING_FS (uint8_t*)(''CDC Config'')
#define USBD_INTERFACE_STRING_FS (uint8_t*)(''CDC Interface'')�?�?�?�?�?�?�?�?�?�?�?

Thanks in advance an let me know if you need any further details!

#cubemx-4.22
This topic has been closed for replies.

3 replies

martonmiklos
Senior
June 7, 2018
Posted on June 07, 2018 at 10:59

Hi ST guys/girls,

Any feedback, concerns regarding to this one?

Nawres GHARBI
ST Technical Moderator
June 27, 2018
Posted on June 27, 2018 at 15:29

Hi Maton, 

I'm not able for the moment to reproduce your issue with TrueStudio and SW4STM32, could you please share your ioc it will be helpful for debug.

Khouloud GARSI
ST Employee
June 7, 2018
Posted on June 07, 2018 at 11:18

Hi

Marton.Miklos

‌,

This is also reported internally for further check.

We really appreciate your contribution to the enhancement of our STM32

resources.

Khouloud.