Skip to main content
danielbuga9
Associate III
July 14, 2017
Question

CubeL4 missing CMSIS

  • July 14, 2017
  • 2 replies
  • 653 views
Posted on July 14, 2017 at 10:21

Hi!

I've migrated one of my projects to CubeL4 v1.8.1 and regenerated my configuration using CubeMX. After that, my project did not compile and I noticed that the cmsis drivers were missing. After a bit of investigation, I found that the firmware package zip file is about 200MB smaller than 1.7 and 1.8 and the uncompressed size is about half, only the ST-specific things are included. That means, there are no third party packages in the L4 patch, no utilities, not even BSP files. This means, that the L4 package is unusable, I had to revert to 1.8.0.

#bug #cubel4
This topic has been closed for replies.

2 replies

danielbuga9
Associate III
July 14, 2017
Posted on July 14, 2017 at 10:33

Note to others who have the same issue: delete and redownload the patch, it solved the issue for me. For whatever reason, the patching process forgot to copy old unchanged files into the 1.8.1 firmware folder...

Khouloud GARSI
ST Employee
July 28, 2017
Posted on July 28, 2017 at 17:57

Dear

Buga.D_niel

‌,

The issue is already reported internally and will be fixed as soon as possible.

Thanks a lot for your contribution to the enhancement of our resources and for sharing the solution with other 'STM32 MCUs forum' users.

Khouloud.