Skip to main content
Mutlu.Mert
Associate II
April 13, 2018
Question

STM32L053 Internal Crystal

  • April 13, 2018
  • 0 replies
  • 378 views
Posted on April 13, 2018 at 18:26

Hi, i want to use internal crystal. I'did configrations via cube mx however it did not worked. I want to test it with blink led. As you see my code;

I don't know where i am wrong ? 

Thanks a lot 

/********************************************

int main( void )

{

bool isMaster = true;

uint8_t i;

HAL_Init( );

SystemClock_Config( );

MX_GPIO_Init();

//*

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_9, GPIO_PIN_SET); //led pin

delay_main=0;

while(delay_main<100);

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_9, GPIO_PIN_RESET);

//*

DBG_Init( );

HW_Init( );

//**

USE_BAND_868;

USE_MODEM_LORA;

//**

/* Led Timers*/

TimerInit(&timerLed, OnledEvent);

TimerSetValue( &timerLed, LED_PERIOD_MS);

TimerStart(&timerLed );

//***************************

And this is my SystemClock_Config task; 

void SystemClock_Config(void)

{

RCC_OscInitTypeDef RCC_OscInitStruct;

RCC_ClkInitTypeDef RCC_ClkInitStruct;

/**Configure the main internal regulator output voltage

*/

__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

/**Initializes the CPU, AHB and APB busses clocks

*/

RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_MSI;

RCC_OscInitStruct.MSIState = RCC_MSI_ON;

RCC_OscInitStruct.MSICalibrationValue = 0;

RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_5;

RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;

if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)

{

Error_Handler();

// _Error_Handler(__FILE__, __LINE__);

}

/**Initializes the CPU, AHB and APB busses clocks

*/

RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK

|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;

RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_MSI;

RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;

RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;

RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;

if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)

{

Error_Handler();

// _Error_Handler(__FILE__, __LINE__);

}

/**Configure the Systick interrupt time

*/

HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);//1000

/**Configure the Systick

*/

HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);

/* SysTick_IRQn interrupt configuration */

HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);

}
    This topic has been closed for replies.