Maximum output current value of PWM, TIM
Sorry for my poor English.
What is the maximum output current value of PWM using TIM? Where can I find it in the data sheet? I am using STM32F334. I am investigating whether the MOSFET can be directly driven by the PWM from the microcomputer without the gate driver.
On page 78/121 of the data sheet of STM32F334x4 STM32F334x6 STM32F334x8, the following description was given

Is IIO=8mA, 20mA the PWM maximum output current value? Which is 8 mA or 20 mA?
Best Regards,
Ken Inoue