Skip to main content
Ken Inoue
Associate III
November 28, 2017
Solved

What is the device address of the M24LR64 - R?

  • November 28, 2017
  • 2 replies
  • 870 views
Posted on November 28, 2017 at 07:05

What is the device address of the M24LR64 - R? I am studying I2C using X-NUCLEO-NFC 02 A 1. X-NUCLEO-NFC02A1 has EEPROM (M24LR64-R). However, I do not know the device address of the M24LR64 - R. Even if I looked at the data sheet, I could not understand where it is written because of beginners. I am happy if you give me a hint.

Best Regards,

Ken Inoue

    This topic has been closed for replies.
    Best answer by AvaTar
    Posted on November 28, 2017 at 09:10

    Does the X-NUCLEO-NFC02A1 user manual say something about it ?

    Checking the M24LR64-R datasheet,it says:

    The device select code consists of a 4-bit device type identifier, and a 3-bit Chip Enable “Address� (E2, E1, E0). To address the memory array, the 4-bit device type identifier is 1010b.

    Address bits E1 and E0 are defined by external pins, so check the schematics.

    E2 depends on the memory range you want to access.

    2 replies

    AvaTar
    AvaTarBest answer
    Senior III
    November 28, 2017
    Posted on November 28, 2017 at 09:10

    Does the X-NUCLEO-NFC02A1 user manual say something about it ?

    Checking the M24LR64-R datasheet,it says:

    The device select code consists of a 4-bit device type identifier, and a 3-bit Chip Enable “Address� (E2, E1, E0). To address the memory array, the 4-bit device type identifier is 1010b.

    Address bits E1 and E0 are defined by external pins, so check the schematics.

    E2 depends on the memory range you want to access.

    Ken Inoue
    Ken InoueAuthor
    Associate III
    November 30, 2017
    Posted on November 30, 2017 at 09:21

    Dear Mr./Ms. AvaTar

    Thanks to you I understood.

    Thanks.

    Best Regards,

    Ken Inoue