Skip to main content
Ken Inoue
Associate III
April 16, 2017
Solved

Please tell me how to calculate the dead time or determine dead time in this figure. 

  • April 16, 2017
  • 5 replies
  • 5266 views
Posted on April 16, 2017 at 17:39

Thank you for your patronage.  Please tell me how to calculate the dead time or determine dead time in this figure. 

I understand that

HCLK = 84MHz

Prescaler = 83

Counter Period = 99

Pulse = 20

Dead Time = 150

so frequency = 10kHz, Duty ratio = 20%. 

But I can't understand dead time is 2?s.

#dead-time
    This topic has been closed for replies.
    Best answer by Haris Riaz
    Posted on April 19, 2017 at 00:20

    Basically it should be like 1/84000000 = 11.9ns. So you can have deadtime between 0 and 1511ns (11.9*127) with 11.9ns steps.

    So for 2us, deadtime value should be like 168. 

    Thats what i think.

    5 replies

    Tesla DeLorean
    Guru
    April 17, 2017
    Posted on April 17, 2017 at 02:16

    No dead time is defined

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Ken Inoue
    Ken InoueAuthor
    Associate III
    April 17, 2017
    Posted on April 17, 2017 at 10:58

    I'm sorry. Dead time =150.

    Haris Riaz
    Haris RiazBest answer
    Visitor II
    April 18, 2017
    Posted on April 19, 2017 at 00:20

    Basically it should be like 1/84000000 = 11.9ns. So you can have deadtime between 0 and 1511ns (11.9*127) with 11.9ns steps.

    So for 2us, deadtime value should be like 168. 

    Thats what i think.

    Haris Riaz
    Visitor II
    April 19, 2017
    Posted on April 19, 2017 at 00:21

    this assumes Tdts = internal clock..

    Ken Inoue
    Ken InoueAuthor
    Associate III
    April 20, 2017
    Posted on April 20, 2017 at 11:24

    Thank you very much.