Skip to main content
kyrreaa
Associate III
May 3, 2018
Question

STM32F103c8t6 - fast interleaved ADC gives samples in wrong order?

  • May 3, 2018
  • 4 replies
  • 2156 views
Posted on May 03, 2018 at 23:53

Using ADC1 and ADC2 in fast interleaved mode with dma transfering 32bit from ADC1.DR to memory in 32 bit device and mem mode (to handle both ADC1 and ADC2 data simultaneously as pr RM0008 and AN3116) delivers data that when plotted seems to be swapped.

RM0008 

sais the lower halfword will be ADC1 data and upper halfword will be ADC2 data. It also states ADC2 will start first and EOC interrupt will be generated by ADC1 which makes sence in that 2 samples are ten transfered every dma cycle in synch with ADC1.

Since the DMA can only increment memory and not decrement the data is thus listed like this when viewing the memory as array of 16 bit samples:

sample 2 (adc1 sample 1)

sample 1 (adc2 sample 1)

sample 4 (adc1 sample 2)

sample 3 (adc2 sample 2)

sample 6 (adc1 sample 3)

sample 5 (adc2 sample 3)

I tested by capturing a sinewave and it looks like sonic the hedgehog...

Swapping buffer[0] with buffer[1], buffer[2] with buffer[3] and so on plots a nice wave.

I cannot find this in the errata as it does exactly as described. It is however not very useful...

Is there a workaround for this?

Am I triggering my ADC's wrong?

I am triggering the start of conversion in a odd way as I am using TIM1 slaved by TIM4 to generate a n-pulse train every 1ms and then using the end of the pulses as trigger for TIM3 which is just to collect the event and synchronize start of ADC since ADC1 cannot listen to TIM1_UPD which is generated when it reaches pulse count 0. (ADC can trigger regular channel conversion from T3_TRGO though, and using TIM3 I can have it trigger on TIM1_TRGO and deliver it's enable as T3_TRGO. I do not see how this can mess things up but you never know...

#dual-fast-interleaved #adc-configuration #dual-interleaved #bluepill #stm32f103
This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
May 4, 2018
Posted on May 04, 2018 at 03:03

Make sure not to do calibration with DMA enabled.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
kyrreaa
kyrreaaAuthor
Associate III
May 4, 2018
Posted on May 04, 2018 at 09:36

I have not run calib with DMA enabled.

A few things I have tested:

- Run with ADCCLK of 4.5 12 and 14 MHz in addition to pushing it to 18 and 36 MHz. Same result.

- Tried enabling only dma on ADC1 or both ADC1 and ADC2. Again no difference. Infact it transfers data fine with DMA only enabled on ADC1.

- Tested DMA transfer widths of 32 to 16 etc. Does not work. (Didn't expect it to.)

- Made sure buffer is 4-byte aligned in memory for proper DMA access.

It's also worth pointing out I am running with no external memory and no other DMA active.

I am also not using any interrupts, just spinning in main waiting long enough for this capture to finish.

Chip revision of my STM32F103C8T6 is X with Marked 'GH235 93 CHN 611'.

MLore.9
Visitor II
December 3, 2018

Yes confirmed the order is shifted. Check AN3116 it says while ADC1 samples the channel, ADC2 converts the previous samples. So actually (also from the picture in this doc) ADC2 start first, then ADC1 is shifted and start after.

MLore.9
Visitor II
December 3, 2018