Skip to main content
deokar
Associate
October 3, 2017
Question

Minimum input voltage for stm32f0

  • October 3, 2017
  • 3 replies
  • 1545 views
Posted on October 03, 2017 at 09:56

Hello ST community,

What if I provide 2.8V as a Vcc to STM32F0? Does it behave properly?

Yes, I have checked input voltage range is 2.4V to 3.6V, still wanted to confirm with you because usually we provide 3.3V to such �Cs.

Thank you for your replies.

#vin #stm-32
    This topic has been closed for replies.

    3 replies

    Nesrine M_O
    Associate
    October 3, 2017
    Posted on October 03, 2017 at 11:02

    Hi

    DEOKAR.Mandar

    ,

    Please try to refer toGeneral operating conditions table in your related datasheet.

    -Nesrine-

    emalund
    Associate III
    October 3, 2017
    Posted on October 03, 2017 at 21:16

    your post is confusing.  do you discuss Vcc or input to a pin?

    Tesla DeLorean
    Guru
    October 3, 2017
    Posted on October 03, 2017 at 23:03

    Yes, you can run the device at 2.8V, most of the DISCO boards run the parts at 3.0V

    As voltages drop you want to be aware of FLASH speed, and USB driver requirements, along with the voltages used by the other parts you are connecting too.

    Review the Data Sheet and Reference Manuals

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..