Skip to main content
autukuri
Associate II
July 25, 2008
Question

USB control transfer questions

  • July 25, 2008
  • 3 replies
  • 652 views
Posted on July 25, 2008 at 18:55

USB control transfer questions

    This topic has been closed for replies.

    3 replies

    autukuri
    autukuriAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:40

    Hello,

    I just started working with the Cortex and had a question on the USB HID control transfer.

    I am working with the ST CUSTOM HID demo application. I am trying to implement GET_REPORT and SET_REPORT functionality to configure my device. I am having difficulty as to where in the code I can insert my routines to process GET and SET_REPORT. Can anyone point me to any example code or project that implements these transfers using ST's USB libraries?

    Thanks in advance.

    autukuri
    autukuriAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:40

    Hey, Thanks for the info. Unfortunately, this USB demo application is the one that I am currently working with. I was surprised to see that none of the demos included support or implement HID control requests such as SET and GET_REPORT. Specifically, I notice that the CUSTOM_HID demo defines FEATURE reports in the HID descriptors, but there is no code that I can see that implements the processing of these packets.

    I am assuming that the functions CustomHID_Data_Setup and CustomHID_NoData_Setup in usb_prop.c is where you would parse report requests, but my attempts so far have been unsuccessful. Maybe I am missing something?

    Thanks!

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:40

    Hi,

    STM32 has a full package on USB and HID custom demos :

    PC Software part :

    http://www.st.com/stonline/products/support/micro/files/um0551.zip

    http://www.st.com/stonline/products/literature/um/14711.pdf (Manual)

    STM32 Firmware Part

    http://www.st.com/stonline/products/support/micro/files/um0424.zip

    http://www.st.com/stonline/products/literature/um/13465.pdf ( Manual)

    Enjoy ! ;)

    STOne-32.