Skip to main content
lil-vince
Associate III
July 10, 2009
Question

Reset state for JTAG pins

  • July 10, 2009
  • 1 reply
  • 829 views
Posted on July 10, 2009 at 13:18

Reset state for JTAG pins

    This topic has been closed for replies.

    1 reply

    lil-vince
    lil-vinceAuthor
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 13:17

    Hi all,

    I´ve seen on the reference manual in GPIO section that:

    Quote:

    The JTAG pins are in input PU/PD after reset:

    PA15: JTDI in PU

    PA14: JTCK in PD

    PA13: JTMS in PU

    PB4: JNTRST in PU

    If I understand correctly, it´s that for example for PA15: MODE=00b(classic reset state input), CNF=10b (input pul-up/down) and ODR=1b(pull-UP)

    Am I right?

    But it´s not mentioned the reset state of PB3 (JTDO)...

    I would like to write directly in this registers without read before like that:

    GPIOB->CRL = vu32(GPIO_CRL_MODE0_0 + GPIO_CRL_CNF4_1 + GPIO_CRL_MODE5_1 + GPIO_CRL_MODE7_1); //only for example

    But I want to use the JTAG and so not to disable it!

    (I haven´t yet my board and so I can´t read the reset state of JTAGs pins)

    Regards,

    Vince

    [ This message was edited by: lil-vince on 10-07-2009 17:24 ]