Skip to main content
md1
Associate III
February 27, 2007
Question

SSPx frequency calculation error

  • February 27, 2007
  • 2 replies
  • 842 views
Posted on February 27, 2007 at 18:13

SSPx frequency calculation error

This topic has been closed for replies.

2 replies

gu48bz
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:36

While on this general area I reported a bug while back which is pretty fundamental in the HAL. Never sure if my bug reports make it to the relevant people, so...

code snipit from 91x_ssp.c...

/* Configure the Mode */

if(SSP_InitStruct->SSP_Mode == SSP_Mode_Slave)

{

/* Set the slave mode */

SSPx->CR1 |= SSP_Mode_Slave;

/* Configure the Slave output */

if(SSP_InitStruct->SSP_SlaveOutput == SSP_SlaveOutput_Disable)

{

/* Slave output disabled */

SSPx->CR1 |= SSP_SlaveOutput_Disable;

}

else

{

/* Slave output enabled */

SSPx->CR1 &= SSP_SlaveOutput_Enable;

}

}

else

{

/* Set the master mode */

SSPx->CR1 &= SSP_Mode_Master;

/* Clear clock rate SCR[7:0] bits */

SSPx->CR0 &= SSP_ClockRate_Mask;

/* Set the serial clock rate */

SSPx->CR0 |= (SSP_InitStruct->SSP_ClockRate<

/* Clear clock prescaler CPSDVSR[7:0] bits */

SSPx->PR &= SSP_ClockPrescaler_Mask; // WRONG, applicable to slave mode as well

/* Set the serial clock prescaler */

SSPx->PR |= SSP_InitStruct->SSP_ClockPrescaler; // WRONG, applicable to slave mode as well

}

SSPx->PR only gets set up in master mode, but not in slave. The consequences on Rev D silicon are pretty harsh. random reboots, ARM core total lockups, total loss of JTAG comms, it's major league stuff.

Also as a side note, running at a PCLK of 96MHz just doesn't fly with the SSP peripheral, it's unstable. 48MHz is far more friendly.

md1
md1Author
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:36

Hi,

I think there may be a slight error in rev1 of the reference manual.

In section 10.4.6 (page 238), the following is quoted:

Quote:

The serial bit rate is derived by dividing down the input clock PCLK. The clock is first divided by

an even prescale value CPSDVSR from 2 to 254, which is programmed in SSP_PR. The clock

is further divided by a value from 1 to 256, which is 1 + SCR, where SCR is the value

programmed in SSP_CR0.

The frequency of the output signal bit clock SCLK is defined below:

fSCLK=fPCLK / (CPSDVR + (1+SCR))

For example, if PCLK is 3.6864MHz, and CPSDVSR = 2, then SCLK has a frequency range

from 7.2kHz to 1.8432MHz.

However, I think the formula should read fSCLK=fPCLK / (CPSDVR x (1+SCR)) to obtain the frequency range specified?

Martin.