Skip to main content
juergen239955
Associate II
January 18, 2007
Question

ST10F269 doesn't work after reset

  • January 18, 2007
  • 8 replies
  • 1689 views
Posted on January 18, 2007 at 09:31

ST10F269 doesn't work after reset

This topic has been closed for replies.

8 replies

juergen239955
Associate II
January 8, 2007
Posted on January 08, 2007 at 12:40

Hi,

I have following problem:

My microcontroller and the program on it work very well. But when I reset it with a short low level on RSTIN pin it doesn't start again and pin RSTOUT stays low.

Can someone help me?

juergen239955
Associate II
January 9, 2007
Posted on January 09, 2007 at 12:04

Hi Neila,

the hardware on RPD is like in the data sheet (R0 = 1M, C0 = 10uF).

The duration of the hardware reset pulse is half a second or longer.

The level on RPD at rising edge of RSTIN is 0V.

The level on EA at rising edge of RSTIN is 5.0V.

The level on P0L.4 at rising edge of RSTIN is 2.5V. (Is this too less?)

Regards,

Juergen

juergen239955
Associate II
January 9, 2007
Posted on January 09, 2007 at 12:36

... I have to correct my last answer: The level on P0L.4 at rising edge of RSTIN is 5.0V and after 150us 2.5V (there is an FPGA with 2.5V which influences this signal).

juergen239955
Associate II
January 11, 2007
Posted on January 11, 2007 at 07:23

Hi Neila,

I will try it with the other values.

I need the BSL mode only to download the program onto the internal flash. But I don't need it in this case.

SYSCON is 0414h.

After reset it never works. After power up it works most times (this means to 95%) but I think that this has the same reason.

Regards,

Juergen

juergen239955
Associate II
January 15, 2007
Posted on January 15, 2007 at 04:27

... now I have tried it with the other values but this had no effect. :-[

juergen239955
Associate II
January 16, 2007
Posted on January 16, 2007 at 05:09

Have you or someone else any other idea?

fweld9
Associate
January 16, 2007
Posted on January 16, 2007 at 06:02

Hi Jürgen,

I remember having observed occasional failures at normal power-up like you.

Maybe it helps you: I found out that when I used a different supply the problem got worse. The normal config was a small switching regulator on board, when I used a laboratory psu instead it resulted in about 50% failure.

Experimenting with the RPD, EA or RSTIN configuration looks fishy to me. Up to now I could not see any reliable solution in any other thread!

Other MCUs can start reliable - ST is challenged in this case - we're only waisting a lot of time on this issue :-(.

Manitux :-?

juergen239955
Associate II
January 18, 2007
Posted on January 18, 2007 at 09:31

Hi Manitux,

that's really strange.

But I use this MCU on two other pcbs, too. And here I don't have any problems with power up. Only on this board. Ok, here I use only a laboratory psu for power supply and not a dc/dc-converter like on the other boards. But when I tried the dc/dc converter solution on the non-working pcb I had the same effect. So, I think, this can't have something to do with the power supply.

Additionally I have to say that I have this problem only when I switch the power supply off and on very fast (half a second or less). When I wait one second (or longer) between switching off and on I never have this problem. And I have this effect always when I reset the MCU. That is the second reason why this can't have something to do with the power supply.

What I think is that the MCU goes into the BSL mode after reset (or power up) but I don't know why (see the other posts above). :-?

Regards,

Juergen