Question
Memory-Loader error
Posted on April 12, 2017 at 15:22
Hi all,
I am facing some issues here on flash erasing and programming. I am not getting where is the actual problem. I am using STM32F429ZET on our custom board. For testing purpose is used provided blinky example's hex file which support same controller. Problem here is that when i am trying to program this hex file using ST-Link utility it throws errors as:
18:22:34 : ST-LINK SN : 49FF70065178505057391687
18:22:34 : ST-LINK Firmware version : V2J28S618:22:34 : Connected via SWD.18:22:34 : SWD Frequency = 4,0 MHz.18:22:34 : Connection mode : Normal.18:22:34 : Debug in Low Power mode enabled.18:22:34 : Device ID:0x419 18:22:34 : Device flash Size : 512KBytes18:22:34 : Device family :STM32F42xxx/F43xxx18:23:04 : [Blinky.hex] opened successfully.18:23:04 : [Blinky.hex] checksum : 0x000F72B6 18:23:07 : Memory-Loader error18:23:07 : Error occured during erase operation!18:23:07 : Programmed memory Checksum: 0x00000000Any idea?
Any suggestions might help me.