Skip to main content
anton23
Associate II
June 11, 2017
Question

Usart 2 does not work

  • June 11, 2017
  • 3 replies
  • 966 views
Posted on June 11, 2017 at 20:31

I am trying to use 2 usart in my program. When i am trying send_to_uart2('a'); nothing happens. In debug mode USART2->SR is always 0x000. Why?

#include 'stm32f10x.h'

#include 'stm32f10x_gpio.h'

#include 'stm32f10x_rcc.h'

void Delay(void)

{

volatile uint32_t i;

for (i = 0; i != 0x140000; i++)

;

}

void send_to_uart1(uint8_t data)

{

while (!(USART1->SR & USART_SR_TC))

;

USART1->DR = data;

}

void send_to_uart2(uint8_t data)

{

while (!(USART2->SR & USART_SR_TC))

;

USART2->DR = data;

}

uint8_t uart_data;

int main(void)

{

GPIO_InitTypeDef PORTA_init_struct;

RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA | RCC_APB2Periph_USART1 | RCC_APB1Periph_USART2, ENABLE);

PORTA_init_struct.GPIO_Pin = GPIO_Pin_9;

PORTA_init_struct.GPIO_Speed = GPIO_Speed_50MHz;

PORTA_init_struct.GPIO_Mode = GPIO_Mode_AF_PP;

GPIO_Init(GPIOA, &PORTA_init_struct);

PORTA_init_struct.GPIO_Pin = GPIO_Pin_10;

PORTA_init_struct.GPIO_Speed = GPIO_Speed_50MHz;

PORTA_init_struct.GPIO_Mode = GPIO_Mode_IN_FLOATING;

GPIO_Init(GPIOA, &PORTA_init_struct);

PORTA_init_struct.GPIO_Pin = GPIO_Pin_2;

PORTA_init_struct.GPIO_Speed = GPIO_Speed_50MHz;

PORTA_init_struct.GPIO_Mode = GPIO_Mode_AF_PP;

GPIO_Init(GPIOB, &PORTA_init_struct);

PORTA_init_struct.GPIO_Pin = GPIO_Pin_3;

PORTA_init_struct.GPIO_Speed = GPIO_Speed_50MHz;

PORTA_init_struct.GPIO_Mode = GPIO_Mode_IN_FLOATING;

GPIO_Init(GPIOA, &PORTA_init_struct);

USART_InitTypeDef uart_struct1;

uart_struct1.USART_BaudRate = 9600;

uart_struct1.USART_WordLength = USART_WordLength_8b;

uart_struct1.USART_StopBits = USART_StopBits_1;

uart_struct1.USART_Parity = USART_Parity_No;

uart_struct1.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

uart_struct1.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

USART_Init(USART1, &uart_struct1);

USART_Cmd(USART1, ENABLE);

USART_InitTypeDef uart_struct2;

uart_struct2.USART_BaudRate = 9600;

uart_struct2.USART_WordLength = USART_WordLength_8b;

uart_struct2.USART_StopBits = USART_StopBits_1;

uart_struct2.USART_Parity = USART_Parity_No;

uart_struct2.USART_HardwareFlowControl = USART_HardwareFlowControl_None;

uart_struct2.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

USART_Init(USART2, &uart_struct2);

USART_Cmd(USART2, ENABLE);

while (1) {

send_to_uart2('a');

Delay();

send_to_uart1('b');

Delay();

}

}
    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    June 11, 2017
    Posted on June 11, 2017 at 20:48

    >>Why?

    USART2 is on APB1, not APB2, enable the right clock

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    anton23
    anton23Author
    Associate II
    June 11, 2017
    Posted on June 11, 2017 at 21:20

    I chaged to 

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART2, ENABLE);

    But it do not work. value  USART2->DR do not change.

    Tesla DeLorean
    Guru
    June 11, 2017
    Posted on June 11, 2017 at 22:33

    The question asked about USART2->SR, which presumably now isn't zero?

    Reading USART2->DR shows the content of the Reception register, it isn't the same thing as the Transmission register you write too, it is not a memory cell.

    Avoid sitting the debugger over the USART, it will alter its behaviour, reading the DR will clear bits in the SR

    If you want to read the same data back in DR, then loop the TX and RX together externally.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..