Skip to main content
mr2399
Visitor II
September 2, 2016
Question

STM32CubeMX - Power Consumption Calculator

  • September 2, 2016
  • 2 replies
  • 3002 views
Posted on September 02, 2016 at 13:38

Hi,

is there the possibility to change the ''Vdd Power Supply'' values inside of the Parameter Selection. I would like to select 2.8V but doesn't have the possibility to do so. Also small file hacks are welcome...

Thanks in advance.

    This topic has been closed for replies.

    2 replies

    Nesrine M_O
    Associate
    September 2, 2016
    Posted on September 02, 2016 at 17:08

    Hi banjoBazooka,

    The power consumption calculator (PCC) in STM32CubeMX returns Average of current consumption, Battery life… these data are taken from the MCU datasheet or interpolated from a user specified bus or core frequency.

    VDD parameter is fixed according to VDD values presented on datasheets.

    Otherwise I will raise this request to our MX team as enhancement.

    -Syrine-
    Bino
    ST Employee
    September 5, 2016
    Posted on September 05, 2016 at 09:53

    Hello,

    Could you please tell us the MCU Name you are using?

    Thanks

    /Eric