TIM2 Upcounting Count Restart Issue
The TIM2 timer on an STM32F0 seems to not be resetting to 0 once the counter reaches the ARR value on occasion. I am periodically changing the ARR value, but the values are all in a small range. After a random amount of cycles, the counter will increment beyond that range without triggering an update event, resetting the counter back to 0. I have tried this with and without TIM_CR1_URS set. TIM_CR1_UDIS bit is in the reset state. Anyone else run into this problem?