Skip to main content
Md Mubdiul Hasan
Associate III
Oct 24, 2016 4:24 AM UTC
Question

Unidirectional receive-only mode SPI using STM32F07xxx

Posted on October 24, 2016 at 06:24

Dear All,

Kindly help me to SPI receive only mode in this structure when I am using SPI1_IRQHandler, is it proper code to apply?

 void SPI1_IRQHandler(void)

   {

     //* SPI in Slave Receiver mode--------------------------------------- */

     if (SPI_I2S_GetITStatus(SPI1, SPI_I2S_IT_RXNE) == SET)

     {

                   /*------- Master --> Slave */

       if (CmdStatus == 0x00)

      {

             CmdReceived = SPI1_RXDR8;

                     Rx_Idx=0;

                     Tx_Idx=0;

                     switch(CmdReceived){

                         case 0x01:

                               receiveSPI=0x01;

                               CmdStatus = 0x01;

                               StartSend=0x00;

                               Cpt_Spi=0;

                             break;

                             case 0x81 :

                                     SendSPI=0x01;

                                     CmdStatus = 0x01;

                                     Spi_Case=0x01;

                                     if (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) != RESET)//wait for TXE = 1

                       SPI1_RXDR8=SPI_Tx1[Tx_Idx++];   // prepare the first byte to be send when the clock is received

                             break;

                             case 0x84:

                                     SendSPI=0x01;

                                     Spi_Case=0x02;

                                     CmdStatus = 0x01;

                                     if (SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE) != RESET)

                        SPI1_RXDR8=SPI_Tx2[Tx_Idx++];  //  // prepare the first byte to be send when the clock is received

                               }

                             break;

                             default:

                                SendSPI=0x00;

                    Spi_Case=0x00;

                    CmdStatus = 0x00;

                    receiveSPI=0x00;

                             break;

                           }// end of switch

             }// end of cmdStatus =0x00

             else

         {

               if(receiveSPI)  // in this case the slave receives data from the master

               {

              SPI_Rx[Rx_Idx++] = SPI1_RXDR8;  // the array sent by the Master in the receive mode

               } // end of receiveSPI

Before that I have been using following functions, 

1. static void MX_DMA_Init(void)

2.static void MX_SPI1_Init(void)

3.void DMA_beginWrite()

4.void DMA1_Stream3_IRQHandler()

5. void SysTick_Handler(void)

    This topic has been closed for replies.