Skip to main content
Nickelgrass
Senior
September 18, 2016
Question

Trouble with RTC and 1Hz interrupt

  • September 18, 2016
  • 3 replies
  • 994 views
Posted on September 18, 2016 at 09:40

Hello,

I have been hanging on this problem since days and have googeld a very lot but can not solve this.

I am working with a Nucleo F411RE and TrueStudio. I want to generate a 1Hz interrupt with the RTC. The system is running and the RTC is nicely running too. I can see the Seconds count and it is very accurate holding the time. So I assume that all is configured correctly regarding the RTC itself. But I can not get the interrupt to work. The WUTIE is set and the WUT is enabled. I checked that all by looking at the register.

I have tryed the Tamp-Stamp-IRQ and the Wakeup-IRQ. But either nothing happens or the interrupt ends up in the ''Infinite_Loop''. 

My code regarding the interrupt setup:

rtc_unlock();

B_OUT(RTC->CR, bit14|bit10|bit2);

rtc_lock();

B_SET(EXTI->IMR, bit22);

B_SET(EXTI->RTSR, bit22);

B_SET(EXTI->SWIER, bit22);

NVIC_SetPriorityGrouping(0);

NVIC_SetPriority(RTC_WKUP_IRQn, 10);

NVIC_EnableIRQ(RTC_WKUP_IRQn);

In the startup_stm32f411xe.s I looked up the funktionname from the RTC_WKUP_IRQHandler and set my IRQhandler to that name. Is there any advice on this, I am getting desperately on this one. How can I get the interrupt to jump into my function? 

void RTC_WKUP_IRQHandler()

{

B_SET(EXTI->PR, bit22);

NUCLEO_LED_ON;

}

Do I have to specify my function somehow to tell the compiler to use it?

Am greatfull for any tips.

Thanks, regards
    This topic has been closed for replies.

    3 replies

    adam23
    Associate II
    September 20, 2016
    Posted on September 20, 2016 at 15:31

    It depends on if you are using any template/example/OS. But yes the address of RTC_WKUP_IRQHandler has to be present in interrupt vector table on right place. It is not placed there ''auto magically''.

    adam23
    Associate II
    September 20, 2016
    Posted on September 20, 2016 at 18:33

    Oh, is the WU not used only for wake up from sleep/standby? From spec of similar STM32

    When the periodic wakeup interrupt is enabled by setting the WUTIE bit in the RTC_CR2 register, it can exit the device from low-power modes.

    The periodic wakeup flag can be routed to the RTC_ALARM output provided it has been enabled through bits OSEL[1:0] of RTC_CR register. RTC_ALARM polarity can be configured through the POL bit in the RTC_CR register.

    So you may have to set the RTC_ALARM...

    Nickelgrass
    Senior
    September 26, 2016
    Posted on September 26, 2016 at 08:20

    Thanks for the reply. Of course i did use the function from the vectortable.

    The hint with the Alarm worked and I simply put the vectortable from the .s file in an own vectortable in a .c file and now I can enter my own function names. 

    Many thanks!