Skip to main content
funkehed
Associate
February 17, 2017
Solved

One ADC channel affecting the other ADC channels STM32F407

  • February 17, 2017
  • 6 replies
  • 4460 views
Posted on February 17, 2017 at 17:56

Hi.

I've been using 4 channel ADC DMA convertion and recently noticed that one of the inputs affects the read values of another. The troubleshouting showed that the voltage on Channel 15(PC5) somehow gets to the other ADC pins.

Interestingly, I see the read values be affected only on one channel (2,PA2). However, I see the voltage change on all other ADC channels when I change voltage on PC5.  With 0.3-3V input swing on PC5, I have almost the same swing on the other ADC pins, if they're not connected to anything, and 8mV swing if the pins connected through opamp buffer and 100ohm.

Did anyone faced a similar problem? This is a second prototype board out of two which exhibits this behaiviour.

void ADC_Config()

{

 

  ADC_InitTypeDef       ADC_InitStructure;

  ADC_CommonInitTypeDef ADC_CommonInitStructure;

  GPIO_InitTypeDef      GPIO_InitStructure;

  DMA_InitTypeDef       DMA_InitStructure;

 

  /* Enable peripheral clocks */

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2 | RCC_AHB1Periph_GPIOA |  RCC_AHB1Periph_GPIOC, ENABLE);

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

   /* DMA2 Stream0 channel0 configuration **************************************/

  DMA_InitStructure.DMA_Channel = DMA_Channel_0;  

  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)&ADC1->DR;;

  DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADCConvertedValues[0];

  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;

  DMA_InitStructure.DMA_BufferSize = 32;

  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Enable;

  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

  DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

  DMA_InitStructure.DMA_Priority = DMA_Priority_High;

  DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;         

  DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;

  DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;

  DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

  DMA_Init(DMA2_Stream0, &DMA_InitStructure);

  DMA_Cmd(DMA2_Stream0, ENABLE);

 

  //DMA_ITConfig(DMA2_Stream0, DMA_IT_TC, ENABLE);

 

  /* Configure ADC pins as analog input */

  GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_1 | GPIO_Pin_2 | GPIO_Pin_3;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;

  GPIO_Init(GPIOA, &GPIO_InitStructure);

 

  GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_5;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

 

  /* ADC Common configuration *************************************************/

  ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;

  ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;

  ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled  ;  

  ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;

  ADC_CommonInit(&ADC_CommonInitStructure);

  /* ADC1 regular channel 1 configuration ************************************/

  ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

  ADC_InitStructure.ADC_ScanConvMode = ENABLE;

  ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;

  ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

  ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

  ADC_InitStructure.ADC_ExternalTrigConv = ADC_ExternalTrigConv_T1_CC1;   // Not used but needed for valid init

  ADC_InitStructure.ADC_NbrOfConversion = 4;

  ADC_Init(ADC1, &ADC_InitStructure);

  ADC_RegularChannelConfig(ADC1, ADC_Channel_15, 1, ADC_SampleTime_28Cycles);

  ADC_RegularChannelConfig(ADC1, ADC_Channel_1, 2, ADC_SampleTime_28Cycles);

  ADC_RegularChannelConfig(ADC1, ADC_Channel_2, 3, ADC_SampleTime_28Cycles);

  ADC_RegularChannelConfig(ADC1, ADC_Channel_3, 4, ADC_SampleTime_28Cycles);

 

 /* Enable DMA request after last transfer (Single-ADC mode) */

  ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);

 

  /* Enable ADC1 DMA */

  ADC_DMACmd(ADC1, ENABLE);

 

 

  /* Enable ADC1 **************************************************************/

  ADC_Cmd(ADC1, ENABLE);

  /* Start ADC1 Software Conversion */

  ADC_SoftwareStartConv(ADC1);

}

#adc #analog-input
This topic has been closed for replies.
Best answer by AvaTar
Posted on February 17, 2017 at 18:04

One ADC with multiplexed channels, and an improper setup. All channels share the same S&H capacitor, explaining this effect.

Either buffer your inputs (opamp) to get a lower impedance, or increase the sample time.

6 replies

AvaTar
AvaTarBest answer
Senior III
February 17, 2017
Posted on February 17, 2017 at 18:04

One ADC with multiplexed channels, and an improper setup. All channels share the same S&H capacitor, explaining this effect.

Either buffer your inputs (opamp) to get a lower impedance, or increase the sample time.

funkehed
funkehedAuthor
Associate
February 17, 2017
Posted on February 17, 2017 at 18:15

The inputs are opamp buffered trough 100ohm ressistors

S.Ma
Principal
February 18, 2017
Posted on February 18, 2017 at 16:23

Play with the adc sample and hold time. Make the integration as small as possible while keeping the output within acceptable noise range. I have seen other solved similar crosstalk like topics in december...