Skip to main content
bjornpaulstrom
Associate II
February 23, 2017
Question

BlueNRG-ms only first bytes of characteristic transfered

  • February 23, 2017
  • 0 replies
  • 487 views
Posted on February 23, 2017 at 18:39

Hello I am using BlueNRG-ms and have a characteristic that is 52 bytes.

However when the client reads it they only get the first 20 something bytes, the rest dont get transfered. Both creating the characteristic and updating its value is successfull according to event complete parameters.

When i did this using the BlueNRG GUI, with the same size and same data it worked...

Char setup:

uint8_t data[] =

{

    HIDServiceHandle[0], HIDServiceHandle[1], //Handle of the service to which the characteristic has to be added

    UUID16BIT, //0x01: 16-bit UUID

   

0x4b, 0x2a, //UUID

   

0x34, 0x00, //Maximum length of the characteristic value

   

PROPERTY_READ, //Bitwise OR values of Characteristic Properties

   

0x00, //0x00: ATTR_PERMISSION_NONE

   

0x01, //0x01: GATT_SERVER_ATTR_WRITE The application will be notified when a client writes to this attribute

   

0x10, //The minimum encryption key size requirement for this attribute. Valid Range: 7 to 16

   

FIXEDLENGTH, //0x00: The attribute has a fixed length value field

};

And the data:

uint8_t data[] =

{

    HIDServiceHandle[0], HIDServiceHandle[1], //Service handle

   

HIDReportMapCharactersiticHandle[0],HIDReportMapCharactersiticHandle[1], //Char handle

   

0x00, //ValueOffset

   

0x34, //Value length

   

0x05,0x01,

   

0x09,0x02,

   

0xA1,0x01,

   

0x09,0x01,

   

0xA1,0x00,

   

0x85,0x01,

   

0x05,0x09,

   

0x19,0x01,

   

0x29,0x03,

   

0x15,0x00,

   

0x25,0x01,

   

0x95,0x03,

   

0x75,0x01,

   

0x81,0x02,

   

0x95,0x01,

   

0x75,0x05,

   

0x81,0x03,

   

0x05,0x01,

   

0x09,0x30,

   

0x09,0x31,

   

0x15,0x81,

   

0x25,0x7F,

   

0x75,0x08,

   

0x95,0x02,

   

0x81,0x06,

   

0xC0,0xC0,

};

#stm32 #bluenrg-ms #hci #ble
This topic has been closed for replies.