Skip to main content
stephengoodman9179
Associate
April 26, 2017
Question

CubeMX 4.20.1 Properties does not appear

  • April 26, 2017
  • 3 replies
  • 752 views
Posted on April 26, 2017 at 21:53

In CubeMX 4.20.1 I have opened a project from a previous version. Then when I go to edit the Properties... no window comes up!  If I open another project or create a new one, the Properties... window appears as expected.

How do I fix this? I need to review and possibly change the properties!

thanks!

    This topic has been closed for replies.

    3 replies

    ST Technical Moderator
    April 27, 2017
    Posted on April 27, 2017 at 11:19

    Hi, 

    Please share your .ioc to check this case.

    Thanks

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Jeanne Joly
    Associate
    May 3, 2017
    Posted on May 03, 2017 at 10:20

    Hello

    Liebman.Mark.002

    ,

    I had a look to your point. I took an ioc from CubeMX4.0 and open it with CubeMX4.1.

    I can open Project/Settings/, open the configuration of IPs etc...

    What do you mean by properties? Is it Project Settings?

    As I can't reproduce the issue and as Imen said, we need you to share your ioc to progress on this point.

    BR. Eric

    stephengoodman9179
    Associate
    May 3, 2017
    Posted on May 03, 2017 at 14:14

    Yes, it was the project settings dialog which would not appear when selected from the menu. In that project it was never seen. If I see it again I will share.