Skip to main content
davedave95
Associate III
December 7, 2016
Question

Origin of ppc-freevle-eabi toolchain?

Posted on December 07, 2016 at 09:13

Hello,

I would like to make a native Linux build of the ppc-freevle-eabi toolchain that is shipped with SPC5Studio; the toolchain comes with a readme.txt with some release notes, but it does not state the origin or where sources can be found.

Can anyone shed some light on this? Are the sources available as a whole, and if not, are the changes made to the default 4.9.2 gcc available somewhere?

Thank you,

    This topic has been closed for replies.

    1 reply

    Erwan YVIN
    ST Technical Moderator
    December 7, 2016
    Posted on December 07, 2016 at 09:57

    Hello Gert ,

    The gcc

    ppc-freevle-eabi toolchain 

    (4.9.2) is coming from NXP-Freescale side.

    the source code is coming from nxp community.

    https://community.nxp.com/docs/DOC-333045

     

    We are using the similar core on PowerPC microcontrollers (MPC56-SPC56)

    Linux version is working well.

               Best regards

                                          Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.