Skip to main content
julius
Associate II
Oct 19, 2016 7:08 AM UTC
Question

Cant read/write from external sdram stm32f429, AS4C8M16S-6TIN

Posted on October 19, 2016 at 09:08

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    11 replies

    waclawek.jan
    Super User
    Oct 19, 2016 9:12 AM UTC
    Posted on October 19, 2016 at 11:12

    A0 and A1 stuck/not connected? Check activity with an oscilloscipe directly on the SDRAM's A0/A1 pins.

    JW
    julius
    juliusAuthor
    Associate II
    Oct 19, 2016 10:24 AM UTC
    Posted on October 19, 2016 at 12:24

    Hi JW,

    good gues, O thought it too. But then blocks of memory would be unredable, because address line is used to send colum and row adress so blocks of memory (4x4 cels) would be the same. Now only repetition 1x4 is the same. To be sure now I ***** signals with oscilloscope. You can see in attach I add A0 compare A1 address line and A1 compare A3 address line. As you can see, everything is fine. Also you can find attach 3, where i higlight adress lines from 0 to

    Today I did one more reseach.

    I noticed that if i continously write/read in SDRAM, sometimes I get values diferent than repeation of 4.

    So write my array

    write[100]and after that I read that array

    read[100]. After read/write i compare these two array and if they not match, I stop writing, and left only reading part.

    Rezult - I always get array with broken repeation 1x4. To be more clear:

    Continously rea/write

    __________________________________________

    Write to sdram Read from sdram (most common)

    0 300

    100 300

    200 300

    300 300

    400 700

    500 700

    600 700

    700 700

    800 1100

    900 1100

    1000 1100

    1100 1100

    1200 1500

    1300 1500

    1400 1500

    1500 1500

    After I capture one mismatch with comon read values i turn of writing

    mismatch After turn of write (only continuous read left)

    300 300

    300 300

    300 300

    300 300

    700 700

    600 600

    600 600

    700 700

    1100 1100

    1100 1100

    1000 1100

    1100 1100

    1500 1500

    1500 1500

    1500 1500

    1500 1500

    So the problem apears only on write sequence.

    Thanks for answer anyway.

    ________________

    Attachments :

    A0_A1.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1KT&d=%2Fa%2F0X0000000blO%2FQ80Fhw8iuywyaFK3MjadTE.Wsqr4GVMQIsLxPf2JgKQ&asPdf=false

    A1_A3.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1DZ&d=%2Fa%2F0X0000000blM%2Fsfs_SrLpjGu1bFNIFoDheRhTbbQAlcWCsB0KMKpuuzk&asPdf=false

    Hardware.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1KJ&d=%2Fa%2F0X0000000blK%2F9qkPM02.O2IH5sbU5tCGjJ1.YLXRIT98iEFKb_h8qrs&asPdf=false
    markus239955_stm1_stmicro_com
    Senior
    Oct 19, 2016 11:49 AM UTC
    Posted on October 19, 2016 at 13:49

    Your SDRAM lacks of sufficient power supply. 100nF capacitors to every VDD and VDDQ pin is necessary, HF Separation of VDD and VDDQ is strongly recommended. To make it even worse in your design, the SDRAM is sharing its 100nF Capacitory with the uC. See the Datasheet of the SDRAM, it draws 200mA during refresh cycle / 120mA in normal use. See attached file to see more Details ...

    ________________

    Attachments :

    SDRAM_Power.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1Fk&d=%2Fa%2F0X0000000blL%2FK1.MxLwTXYbtaa7tqZb4sHWZG9Mr4TrI6oZDHnehO_U&asPdf=false
    markus239955_stm1_stmicro_com
    Senior
    Oct 19, 2016 12:04 PM UTC
    Posted on October 19, 2016 at 14:04

    See also attached schematics of STM32F4/7 Disco SDRAM with extra 100nF Capacitors for every VDD/VDDQ pin.

    ________________

    Attachments :

    SDRAM_DISCO.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1K0&d=%2Fa%2F0X0000000blJ%2F3Y105pHYLKetgaSEHsmZlaoVyfu5HTDRlmKEX2ASEg0&asPdf=false
    julius
    juliusAuthor
    Associate II
    Oct 20, 2016 8:50 AM UTC
    Posted on October 20, 2016 at 10:50

    Hello Markus, thank you for answer,

    I try to connect 100 nF capacitors on each VDD and VDDQ pin (see in attatch). There is no shorts i tested all posible shorts with multimeter. But the result is the same.

    Any more ideas, why this bug is appearing?

    ________________

    Attachments :

    soldered_100n_and_4.7uF_cap.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1K9&d=%2Fa%2F0X0000000blH%2FbsZARaawUCwg26AnVwFTKncHsbzwHHy6gpZzQhxoqV4&asPdf=false
    waclawek.jan
    Super User
    Oct 20, 2016 9:17 AM UTC
    Posted on October 20, 2016 at 11:17

    I'd start with small steps: clear the entire memory (write 0), check it is clear, then write some nonzero value to a single address once, check entire memory for changes. Try with different values and different addresses, but always one write only. Come back with results.

    JW
    julius
    juliusAuthor
    Associate II
    Oct 20, 2016 10:02 AM UTC
    Posted on October 20, 2016 at 12:02

    Hi JW,

    Write zeroes to SDRAM was alredy done by initialization code. Folowing your instructions I implement test code:

     

     write[0]=0xFAFA;

     

     HAL_SDRAM_Write_16b(&g_sdram, 0xD0000000+111112, &write, 1);  // values I tried: 0, 12, 112, 1112, 11112 and 111112

     

     for (i=0; i<0x400000; i+=2)   // 0x400000 - ram size, based on uint16_t words

     

     {

     

      HAL_SDRAM_Read_16b(&g_sdram, 0xD0000000+i, &read, 1);

     

       if (read[0]==0)

     

     read[0]=0;

     

       else if (read[0]!=0xFAFA)

     

     read[0]=read[0];              // breakpoint 1

     

       else if (read[0]==0xFAFA)

     

     read[0]=read[0];             // breakpoint 2

     

     }

     

    Rezult: I always 4 times stoped on breakpoint 2, which indicates writed value in 4 cells after 1 write cycle, and then I get end of the for cycle. Breakpoint 1 newer occured. I do not put breakpoint on first if, because most of memory is zero.

    Note: I have more than one sample, all act the same

    Any ideas?
    waclawek.jan
    Super User
    Oct 20, 2016 10:48 AM UTC
    Posted on October 20, 2016 at 12:48

    I've just noticed:

     

    >  sdramCommand.ModeRegisterDefinition =(uint32_t)  SDRAM_MODEREG_BURST_LENGTH_2             |       

     

     

    I believe FMC does not support bursts on the SDRAM-interface. RM0090 rev.13 in 37.7.3  SDRAM controller functional description, SDRAM initialization checklist, item 7:

     

    The Burst Length (BL) of 1 must be selected by configuring the M[2:0] bits to 000

     

    in the mode register (refer to the SDRAM datasheet).

    Please review. I am no FMC/SDRAM expert.

    JW

    julius
    juliusAuthor
    Associate II
    Oct 20, 2016 11:08 AM UTC
    Posted on October 20, 2016 at 13:08

    Acording to your note, I changed this part to:

     

      sdramCommand.ModeRegisterDefinition =(uint32_t)  SDRAM_MODEREG_BURST_LENGTH_1             | // ((uint16_t)0x0000)

     

                                              SDRAM_MODEREG_BURST_TYPE_SEQUENTIAL      | // ((uint16_t)0x0000)

     

                                                             FMC_SDRAM_CAS_LATENCY_3                  | // ((uint16_t)0x0030)

     

                                                           SDRAM_MODEREG_OPERATING_MODE_STANDARD    | // ((uint16_t)0x0000)

     

                                                             SDRAM_MODEREG_WRITEBURST_MODE_SINGLE;      // ((uint16_t)0x0200)

     

    Unfortunately i get the same rezult. I have also tried to change this row:

      g_sdram.Init.ReadBurst = FMC_SDRAM_RBURST_ENABLE;

     

    But nothing happened.

    Any more ideas?

    waclawek.jan
    Super User
    Oct 20, 2016 11:25 AM UTC
    Posted on October 20, 2016 at 13:25

                                                           FMC_SDRAM_CAS_LATENCY_3                  | // ((uint16_t)0x0030)

     

     

    You probably meant SDRAM_MODEREG_CAS_LATENCY_3 ?

    JW