Skip to main content
marco32
Associate III
March 3, 2004
Question

IR level measure

  • March 3, 2004
  • 2 replies
  • 769 views
Posted on March 03, 2004 at 08:08

IR level measure

This topic has been closed for replies.

2 replies

marco32
marco32Author
Associate III
March 1, 2004
Posted on March 01, 2004 at 11:11

Has anybody made an IR level sensor, or has anybody an application note about it?

I've a lot of noise from daylight and big light sources (150W). How can a eliminate it?

Thanks
kasparov
Associate
March 3, 2004
Posted on March 03, 2004 at 08:08

You are working whit IR, that is in a specific range of frequencies. You can try using an optical filter whit a proper lens which allows only IR passage . Or you can modulate your IR source at a frequency different from a 50Hz multiple and use a lockin amplifier to detect your signal inside noise